המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why does my my S-Flex have no drive display and won't run in AFC or bypass?

Article available in these languages: Spanish

Issue:
My S-Flex has no drive display and won't run in AFC or bypass.

Product Line:
Altivar 212 S-Flex

Environment:
All

Cause:
Isolation contactor won't pull in, can't run in AFC or bypass

Resolution:
Check to see if the overload has tripped. If it's tripped, press the blue reset button.
Review the 120V control circuit for blown fuse, open connection, etc.
Standard S-Flex wiring diagrams are published in the S-Flex Installation and User Guide.
Link Here: https://www.se.com/us/en/download/document/30072-451-83/

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team. If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)