המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
[Video] How to Install Schneider Electric IIoT nodes into the HMIBSC?
Goals and Symptoms
The Magelis Edge Box HMIBSC running with Linux is supplied with Node Red.
It has the possibility, through Node Red, to manage the Analog card used as optional, the GPIO, the Hardware platform and the UPS.  But the nodes dedicated for these components are not preinstalled by default.
These nodes can be installed from the recovery SD Card supplied with the HMIBSC.
The goal of this resolution is to provide the steps to follow in order to install IIoT nodes from the SD Card into the server.
Causes and Fixes
Here is the video to show how to install IIoT nodes from the SD card

Schneider Electric IIoT nodes into the HMIBSC? | שניידר אלקטריק ישראל