המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is there a Raven Black spray paint available for NetShelter cabinets?
Issue:
A customer requests spray paint.

Product Line:
NetShelter SX, SV VX, WX

Environment:
All versions and serial ranges.

Cause:
Minor damage to the paint may require spray paint to cover.

Resolution:

We do not currently offer the Raven Black in spray paint, but we do have it available in a paint pen under part #690-0108-001.
Rust-Oleum has a black spray paint available that, while not a perfect match, can be used. Since it's not a perfect match the painted surface may be visible depending upon the lighting.
The Rust-Oleum part number is 7220830, Textured Black.