איך נוכל לעזור לך היום?

How to configure the IO Mapping for the BMENOP0300 IEC61850 Client

Issue
How to configure the IO Mapping for the BMENOP0300 IEC61850 Client

Product Line
Control Expert, Unity 13.1

Environment
Windows 7, Windows 10, Windows 8

Resolution
This video will demonstrates how to:
  • Create the IO mapping for a BMENOP0300  IEC61850 client using the 'IEC61850 Configuration Tool'.
  • Import the mapped variables into the Unity or Control Expert application.

https://www.youtube.com/watch?v=uUZ2SxjzcHE