המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to uninstall Control Expert Version V14 ( former Unity Pro ) from your PC loaded with Windows 7 or Windows 10 Pro
Issue
Customer wants to uninstall the Control Expert Version V14 from his PC

Product Line
Control Expert V14 ( former Unity Pro )

Environment
Microsoft Windows 10 Pro
Version10.0.17134 Build 17134
or
Windows 7

Resolution
  1. Uninstall Control Expert V14.0 from control panel.
  2. In the computer delete the content of the following folders:
  • C:\ProgramData\Schneider Electric\Control Expert
  • C:\ProgramData\Schneider Electric\CommonControlExpert
  • C:\Program Files (x86)\Schneider Electric\Control Expert
  1. In the registry editor delete the following keys:
  • HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\Control Expert
  • HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\Control ExpertConfCatalog
  • HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\Control ExpertTypesLibrary