המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can the Square D Split Core Current Transformer (CTs) 600 V series be installed on uninsulated bus?
Issue
Installation of the Square D Split Core Current Transformer (CTs) 600 V series on uninsulated bus.

Product Line
Split Core Current Transformer (CT)
PowerLogic and ION meters

Environment
Current Transformer
Energy Meter basic metering

Cause
It is required to know the Square D Split Core Current Transformer (CTs) 600 V series specifications prior installation.
Resolution
The Square D Split Core Current Transformers (CT)  600 V Series single ratio, output 5 A in the secondary, up to 600 V, and are for indoor used. More detail on their technical specifications can be found in the attached Datasheets. See the Square D Instrument Transformer on page 41, as well as on Square D Instrument 600 Volt Class Section 6 Transformers on page 13. Open the files attached below.
The maximum voltage without additional insulation is 600 V ac. Do not apply 600 V class current transformers to circuits measuring phase-to-phase voltage greater than 600 V, unless adequate additional insulation is applied between the primary conductor and the current transformers. Square D assumes no responsibility for damage of equipment or personal injury caused by transformers operated on circuits above their published ratings.
Therefore, the split core current transformer 600 V series can be used in uninsulated bus for voltage less or equal to 600 V as said above.

שניידר אלקטריק ישראל

קבצים מצורפים
Data Sheet Characteristics.pdf [49.25 KB]
Instrument Transformer.pdf [1.06 MB]
Instrument 600 Volt Class.pdf [436.84 KB]
גלה עוד
מוצר:
גלה עוד
מוצר: