המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can the ATV340 keypad (VW3A1113) be used with the Process Drive Mounting kit (VW3A1112)?

Issue:
ATV340 keypad (VW3A1113) compatibility with the Process Drive Mounting kit (VW3A1112)

Product Line:
VW3A1113 and VW3A1112

Environment:
All

Cause:
Installation

Resolution:
This is not recommended. The VW3A1113 will technically fit into the VW3A1112 mounting kit (clamshell); however, it does not clip in so there's nothing holding it in place. Also, there is a gap between the keypad and the mounting kit, which makes it lose its IP rating. The keypad does connect to a drive through the mounting kit, but the slightest jarring or turning of the keypad makes it lose connection. It's recommended to use the VW3A1114 mounting kit, which is designed for the VW3A1113 keypad.

pic1

pic2

pic3

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)