איך נוכל לעזור לך היום?

ATV320- cannot change AI2 to current

Issue:
Why I cannot change AI2 to current on the ATV320?

Product Line:
ATV320


Environment:
All model numbers, all serial numbers


Cause:
n/a


Resolution:
AI2 is ONLY for voltage ( 0-10 or 0 to +/-10v). For 4-20ma input, suggest to use AI3, set to current (4-20ma).
Then go to CTL menu- set Fr1 to AI3