המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to write command word, bits 11-15 to Altivar drive via ecostruxure machine expert software when certain Altivar function and inputs has already association with ecostruxure machine expert?

Article available in these languages: Japanese

If the Altivar drive is added to a PLC via its Altivar DTM (device type manager) then the whole command word (CMD) is managed by ecostruxure machine expert and so function blocks running in machine expert will not allow to write single bit of CMD word.
The only solution today is to add the device as a generic Modbus TCP device (not via Altivar DTM) and configure I/O scanner manually. Then you can write every single bit of CMD word by your machine expert program.