המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can an Ethernet module be added to a "Non-E" version of an ATV340 series drive?
Issue:
Customer has purchased a "non-E" version of the ATV340 drive but needs to communicate with the drive via Ethernet.

Product Line:
Altivar Machines, Altivar 340

Environment:
"Non-E" version of the drive (last digit of part number is NOT an E)

Cause:
Clarification of product capabilities.

Resolution:
No. An ATV340 drive that does not have integrate Ethernet communication options can not have them added via an option card.   There are two versions of the ATV340 series drive, the E and the Non-E.  If Ethernet communication is needed you must purchase the E version (Last digit of part number is E).