המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to connect encoder signals to VW3A3424 HTL encoder card in case the A and B signals are available olny?
VW3A3424 is HTL encoder card used for Altivar Process ATV900
It can work with A, /A, B, /B signals or with A and B only or with A only.
The component signals /A and /B must be connected to the encoder card either 0V or to V+. It depends on the type of encoder signals.
If the encoder is the push-pull type that provides A and B signals, then missing component signals /A and /B must be connected to 0V
Likewise in an open collector encoder if the output signals are of PNP type, missing /A and /B must be connected to 0V.
For NPN type the missing /A and /B must be connected to V+ of the encoder card.

See the highlight on an extracted page from the encoder card instruction sheet.

שניידר אלקטריק ישראל

קבצים מצורפים
Extracted pages from ATV_IS_HTL_Encoder_QGH17640_00.pdf [139.23 KB]