המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Customer wants to have multiple Remote Desktop connection with EcoStruxure™ Control Expert V14?
Issue:
The Customer wants to have multiple Remote Desktop connection with EcoStruxure™ Control Expert V14.

Product Line:
EcoStruxure™ Control Expert V14

Environment:
Server (Windows Server 2016), Clients (Windows 7, Windows 10, etc.)

Resolution:
With the Node-Locked License, only one Remote desktop connection is supported at a time.
With the Floating License, you can have multiple (as much as usage rights are available) remote desktop connections at the same time.