איך נוכל לעזור לך היום?

Control Expert 14 returns 'Unknown fatal exception' error when creating a new application after closing an existing one.

Issue
Control Expert 14 returns 'Unknown fatal exception' error when creating a new application after closing an existing one.

Product Line
Control Expert 14

Environment
Windows 7, windows 8, Windows 10

Resolution
The issue is due to a bad installation of Control Expert.  The following steps can be used to resolve the issue:
  • Backup the saved applications.
  • Uninstall ‘Control Expert 14’
  • Uninstall the ‘EcoStruxture Control Expert PSx DTM Library’
  • Delete the folders that were left behind (C:\Users\Public\Documents\Schneider Electric\Control Expert 14.0)
  • Reboot the PC.
  • Clean out the 'C:\Users\SESA40~1\AppData\Local\Temp' folder.
  • Run a registry cleaner.
  • Reboot he PC
  • Reinstall Control Expert.
  • Retest.
  • Install the hotfixes in order (Run Control Expert after each install of the hotfix.)
  • Retest.