המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
In Ecostruxure Power Build - Rapsody is there anyway to generate terminals for feeders in Single Line Diagram?
Yes, we can generate terminals for feeders in Single Line Diagram.  After the selection of the companents in the product choice tab, move to Electrical organisation tab where the single line diagram can be visualised both in horizontal and vertical displays.
Further to generate terminals, click on the "Generate terminals" button (please refer the snapshot attached to see the button). Automatically Rapsody will generate the terminals.

If the user do not want terminals then click on the "remove terminals" button and automatically software will remove the terminals.