המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How is the Self Test accessed in the ATS22?

Article available in these languages: Czech, Spanish

Issue:
Access Self Test in an ATS22.

Product Line:
Altistart 22

Environment:
All

Cause:
Troubleshooting

Resolution:
Access the Utility Menu by pressing the ESC and the UP arrow buttons at the same time.
Navigate to tESt and press ENT

Result
Good
BAd. Possible causes :
- Improper internal voltage,
- Checksum error,
- Disconnected keyboard,
- Disconnected heatsink thermal sensor,
- Disconnected bypass relay (frame size C).

Refer to the ATS22 User Manual for further details.