המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to update Symbol Link in EOTE V3.1
1. Issue
One customer uses Symbol Link to import variables taken from .smbp file (Machine Expert Basic) to EOTE. In case of the modification on the .smbp file, is it possible to make an update of this link inside EOTE?
2. Environment
EOTE V3.1
3. Resolution
The answer is no. EOTE V3.1 does not support direct Symbol Link update. If you want to do an update, you need to delete the previous link first, then add the symbol link again. R&D team is considering improving this by supporting update symbol link feature in V3.2.