המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Video: How to save and upload configurations within the ATV320 C drive?

Issue:
Saving and uploading parameters on the ATV320 C drive.

Product Line:
Altivar 320

Environment:
All

Cause:
Uploading and download

Resolution:



To save configuration files go into CONF, FCS-, SCS1.
Save to STR1 or STR2 as preferred.

To upload to the VFD, go into CONF, FCS-, FCS1.
Select CFG1 or CFG2 depending on whether the files are saved to STR1 or STR2.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)