המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
is it possible to read the FDR server located inside a CPU of a M580 PLC range
It's not possible to observe it.
The FDR server require login and password which are not available for the public.
However, in case of doubt, contact the technical  support team.
They will escalade a specific case and will reproduce then help you to clarify the situation.

In a M580 Hot-Standby system, Schneider has implemented a DTM menu in "Control Expert" configuration tool which allow to synchronized the FDR server of the Standby CPU with the FDR server of the Primary CPU.