המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do I erase the program in the internal memory of a TSX Micro PLC?

Issue:
Erasing the internal memory of a TSX Micro PLC.


Product Line:
TSX Micro, PL7 Micro


Resolution:
In some cases, it may be useful to totally erase the contents of the internal RAM or FLASH EPROM of the TSX37 PLC. To erase the PLC program, during a power-up keep the DIAG button pressed for a minimum of 10 seconds. After this time the ERR light will flash and the RUN light will be off. This indicates no program is in the PLC memory.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)