המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
For Modbus Serial communication between M241/M251/M262 and Altivar 320 Polarization Resistor?

Issue
For Modbus Serial communication between M241/M251/M262 and Altivar 320, does the Polarization Resistor setting need to be turned on?

Product Line
Altivar 320, Modicon M241, Modicon M251, Modicon M262, EcoStruxure Machine Expert / SoMachine

Environment
Serial Communication setup in PLC configuration software

Resolution
Yes, polarization must be turned on in the PLC as per p27 of the ATV320 Modbus Manual:
(Document Reference#NVE41308)
https://www.se.com/ww/en/download/document/NVE41308/

To apply the setting, in EcoStruxure Machine Expert (or the previous version SoMachine):

  1. In the Devices Tree of your EcoStruxure Machine Expert / SoMachine project, expand the tree for your PLC.
  2. Doubleclick on the Serial_Line_1 (or Serial_Line_2)node
  3. Under "Physical Medium", choose "Yes" in the dropdown list for Polarization Resistor

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)