המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to use Text Display in Vijeo Designer
  1. Issue
How to use Text Display in Vijeo Designer?
  1. Environment
Vijeo Designer 6.2 [SPx].
  1. Resolution
Here is an example to use Text Display in Vijeo Designer.
Step 1. Create two text files as below. Insert two colons to identify the start of a text block.The two colons will not appear in the text display. Select Unicode encoding when saving the file.


Step 2.Add the text files into Text File Editor in Vijeo Designer project .

Step 3.Create 3 variables for Text Display and fill them into Property Inspector window.


Step 4.Simulate to run the project, User will get the result as below.


  1. FAQ Applicable Conditions
FAQ applies to all Vijeo Designer 6.2 SPx.