המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PME - Multiple Billing Report generates a blank report after deleting a virtual meter in Hierarchy Manager

Issue
Running some reports that use Virtual Meters or Layouts such as the Multiple Billing Report generates a blank report with the header "Information Requiring Your Attention". System Log Events shows the error "An error occurred while attempting to retrieve data."

Multiple Billing Report Blank

Product Line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Web Applications

Cause
Deleting a virtual meter in Hierarchy Manager does not automatically remove it from the sources list for any saved reports for which it is selected. It needs to be manually deselected even though it no longer appears as an option under Select Sources.

Resolution

1. Open the Report Inputs for the report the user is trying to generate
2. Click Select Sources
3. Click Clear Selection in the top right corner of this window, it will deselect the deleted virtual meter that is hidden

Source Selector

4. Click OK then Generate Report, it should now populate with data as expected