המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PME 2020 - Report Help Links are broken for many Web Reports - 404 Error
Issue
In the Add Report – Report Template Selection section in PME 2020, some of the Report help link is not working.
For example, Backup Power and Billing reports, when clicking on the Report help link for each of the Report template, it displays 404 Error page.

Product Line
Power Monitoring Expert 2020

Environment
Web Application - Report Help Link

Cause
The linking is pointing to a different location.

Resolution
The navigation within the Help Contents work properly.
This issue will be correct with CU1.