המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the MODBUS Register Mapping of Identity for CPUs and communication modules in M580?
Issue
Customers want to know the mapping of the Identity on CPUs and BMENOC0301/11 communication modules in M580 systems.

Product Line
Ecostruxure Control Expert, Unity Pro, M580, BMENOC0301, BMENOC0311

Environment
Control Expert v14.1, Windows 10 version 1902 (OS Build 18362.30), BMEP586040 v3.10, BMENOC0301 v2.17

Resolution
Identity data of 24 words, are availalble on CPUs and BMENOC0301/11 communication modules using Modbus function code 3 with the unit ID set to 100, offset Modbus Address 2001 and below is the MODBUS Register Mapping:
AddressMS ByteLS ByteCIP TypeComments
2001MS ByteLS ByteUINTVendor ID
Offset + 01MS ByteLS ByteUINTDevice Type
Offset + 02MS ByteLS ByteUINTProduct code
Offset + 03MS ByteLS ByteUSINTRevision – Major Revision
Not used
Offset + 04MS ByteLS ByteUSINTRevision – Minor Revision
Not used
Offset + 05MS ByteLS ByteWORDStatus
Offset + 06MSW – MSBMSW – LSBUDINTSerial Number
Offset + 07LSW – MSBLSW – LSB
Offset + 08MS ByteLS ByteWORDLength of Product Name
Not usedLengthMax of 32 characters
Offset + 09MS byte LS ByteSHORT_Product Name: Length 32 characters
CH 0CH 1STRING
Offset + 09 + 15CH 14CH 15