המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PME Scheduled backup task not deleting old backups

Issue
PME scheduled backup task is not deleting the older backup files as expected

Product line
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022

Cause
‘Backup.ps1’ file contains the number of backup files to retain:
"..\Power Monitoring Expert\config\cfg\DbScheduledTasks\Backup.ps1"

'IONMaintenance' user is the default Windows account that executes the BACKUP tasks in Windows Task Scheduler. 'IONMaintenance' user account needs to have “Modify” permission to the backup directories to be able to delete the older backup files.

Resolution
First, locate the backup directory:
The PowerShell script, Configuration.ps1, contains the configuration information for scheduled tasks related to maintaining the ION databases.
The default path for the configuration file is 'Power Monitoring Expert\config\cfg\DbScheduledTasks\Support\'.

Configuration.ps1 contains the parameter, $locationForBackupFiles, which specifies the location where the backup jobs will save the database backups.

By default this parameter is set to: $locationForBackupFiles = "cfg\DBBackups\"

Therefore, the default location of the database backups is 'Power Monitoring Expert\config\cfg\DBBackups\'.

on the backup directory, the 'IONMaintenance' user account can either be added directly to the list of users or to a group of users.

Resolution 1:
'IONMaintenance' user can be added directly to Backup directory with "Modify" permission:
Right-click on the backup folder > click 'Properties' > choose the 'Security' tab and then click 'Edit'

backup1

In 'Group or User names' panel find and select 'IONMaintenance' user.
In 'Permission for IONMaintenance' panel and check Allow for Modify if it is not already selected.

permissions


If IONMaintenance does not exist in ‘Group or user names’ panel then click 'Add...' the 'Select Users or Groups' window will open. Type 'IONMaintenance' then click 'OK'

IONMaintenance

Select the 'IONMaintenance' user and check ‘Modify' permission then click OK.

Resolution 2:

'IONMaintenance' can be added to an existing Group such as 'Users' or 'Administrator' who might have enough permission on the backup directories.
The procedure to add/modify Group permission is similar to Resolution 1.