המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I find the latest Cumulative Update and .iso files for Power SCADA Operation?

Issue
PSO .iso & Cumulative Update

Product Line

Power Operation 2024 (PO 2024)
Power Operation 2022 (PO 2022)
Power Operation 2021 (PO 2021)
Latest Drivers for Power Operation
Graphics Migration Assistant
Power SCADA Anywhere (compatible with multiple Power Operation versions)
Power SCADA Operation 2020 (PSO 2020)
Power SCADA Operation 9.0 (PSO 9.0)
Power SCADA Expert 8.2 (PSE 8.2)
Power SCADA Expert 8.1 (PSE 8.1)
Power SCADA Expert 8.0 (PSE 8.0)
Power SCADA Expert 7.40 (PSE 7.40)
Power SCADA Expert 7.30 (PSE 7.30)
Power SCADA Expert 7.20 (PSE 7.20)

Environment
All PSO/PSE 2024, 2022, 2021, 2020, 9.0, 8.x, 7.x

Cause
User needs up to date installer, cumulative update or driver file.

Resolution
PSO Installers, Cumulative Updates and Driver

This link goes to the exchange community website. New user will have to create an account to browse the content of this site. Pay attention to the version number when selecting. WARNING once a cumulative update has been installed it cannot be uninstalled.