המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PME9 / PME2020 - Partial dial display scale marking shows junk value in Web App

Issue:
In PME9 the partial-dial-display shows junk value in the scale marking. It happens only with the partial dial display. The full dial display works well. The behavior is the same even with PME2020.

a

It can be reproduced by following these steps.

  1. Open Meter Properties
  2. Set From range either 0 or 1.
  3. Try to set Ticks Major every value to 0.1, 0.2, 0.3
  4. Save the diagram
  5. Check Web App Diagrams.

a

Product Line:
Power Monitoring Expert 9, Power Monitoring Expert 2020

Environment:
Web App - Diagram - Partial Dial Display

Cause:
This is a bug in the PME9 and PME2020.

Workaround:
Till there is a permanent fix for this you may try to set the Major Ticks value something at a higher point to avoid such issues.