המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What features are included in the PME Data Exchange Module license?
Product Line
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
Data Exchange Module License

Resolution
The Data Exchange Module license that was released in PME 2023 includes some existing and new features:
  • OPC DA server
  • Measurement Aggregation Export Report
  • Measurement Statistics Export Report
  • VIP Modbus Slave functionality
  • COMTRADE export with ETL
NOTE: On system upgrade, an existing OPC DA server license is converted automatically to a Data Exchange Module license.

Please check the system guide pertaining to PME version in question under the "Software Modules and Licenses" section for specific changes.