המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Definition of %SW117 for the PLC_STAT word 4 of the PLCSTAT DFB cannot be found in the help.
Issue
Definition of %SW117 listed for the PLC_STAT word 4 of the PLCSTAT DFB cannot be found in the help.

Product Line
Control Expert 14.1

Environment
Windows 10

Resolution
The PLCSTAT DFB from the Extras folder of the Control Expert v14.1 DVD provides the ability to convert the Quantum STAT block to an
M580 PLC STATUS block..  Within the PLCSTAT DFB code, there is a word %SW117 listed for the PLC_STAT word 4.  The help
does not provide a definition of the error codes returned by the Control Expert for word %SW117..


Word %SW117 is used for the RIO status.   The following is a list of definitions for the  error  codes that can be returned by %SW117

RIO STATUS CODE
RIO_ERR_INIT_FAILED             0x0010
RIO_ERR_CRP_HOTSWAP          0x0020
RIO_ERR_DIAG_FAILED            0x0030
RIO_ERR_BAD_STATE               0x0040
RIO_ERR_WRONG_VERS          0x0050
RIO_ERR_BAD_TCOP                0x0060
RIO_ERR_CRP_COM_ERROR     0x0070
RIO_ERR_CRP_MODE               0x0080
RIO_ERR_CRP_TIMEOUT           0x0090