המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to configure Event Watcher to trigger on Sag/Swell events only

Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Event Watcher

Resolution
Event Watcher must be configured to use a template that only references Sag/Swell Events.

To create the template follow the steps below:

  1. Open Event Watcher by going to Management Console, select Tools >> Reporting Configuration >> Event Watcher Manager
  2. Select the Templates tab
  3. Click New
  4. Give the alarm a name such as PQ Events - Sag/Swell
  5. If desired, give the alarm a description
  6. Choose 'Select From Event Log'
  7. Select Sag/Swell {0.EN_US}|1 Disturbance Start SS1 DistState Disturbance
Event watcher template
  1. Press OK and then apply to save the template
Event Watcher with template


Configure Event watcher to use the Sag/Swell template by using the following steps.

  1. Inside of Event Watcher choose the Event Watchers tab.
  2. Select New in the top right
  3. Give the alarm a name
  4. Select the Sag/Swell template created above
  5. If desired, give the alarm a description
  6. Select the device(s) that the alarm will apply to
Select device
  1. Press OK

For steps on how to create a report subscription using this event trigger see FA300069.