המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to set PID preset references for the ATV630 drive?

Article available in these languages: Spanish

Issue:
Can I program drive to switch between different set points on PID controller for the ATV630 drive?

Product Line:
ATV630

Environment:
All models, all serial numbers

Cause:
Customer wanted to easily switch between three set points, 40, 60 and 80 PSI.

Resolution:
Under the main menu, enter complete setting -> Pump Functions -> PID Controller -> PID Reference -> PID preset references:
Assign a digital input (DI5) for 2 PID Preset Assign
Enter 40PSI for RefPID Preset 2
Assign a digital input (DI6) for 4 PID Preset Assign
Enter 60PSI for RefPID Preset 3
Enter 80PSI for RefPID Preset 4

Note: This function can be accessed if [PID feedback ass.] PIF is assigned.