איך נוכל לעזור לך היום?

In IONSetup, Is there any way to view device timestamps in a different time zone than my PC?

A new feature, ION Setup will now attempt to detect a device’s programmed time zone and prompt the user if it is different than the PC.
TimeZone Setup


The automatic time zone detection can be enabled/disabled from the Tools -> Options menu on the View tab.
TimeZone Options


Once set, the selected time zone setting can be modified using the Device Properties -> Time Zone tab.

Device Properties
All UTC time stamps will then use the selected setting when showing device data (meter local time will display as it is).