המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PowerLogic PM3000 Series (PM3200, PM3210, PM3250, PM3255) Installation and User Guide
Issue
PM3000 Series Installation and User Guide

Product Line
PM3200, PM3210, PM3250, PM3255

Environment
Installation, Configuration, Programming, Instruction bulletin, User Manual

Cause
Documentation is needed to configure and install a PM3000 series meter

Resolution
Refer to the attached User Guide, Installation Guide and Technical Datasheet below for PM3200, PM3210, PM3250, and PM3255 series meters.

Refer to Article Where to find the CAD drawings for the PM3000 Power Meter? for CAD drawings.

Refer to the User Guide for the Modbus Register List.

PM3000 Series User Guide and Register List
PM3200, PM3210 Installation Guide
PM3250, PM3255 Installation Guide
PM3000 Series Technical Datasheet

שניידר אלקטריק ישראל

קבצים מצורפים
PM3250, PM3255 Installation Guide 2019.pdf [3.67 MB]
PM3200 Series User Guide 2016.pdf [2.45 MB]
PM3000 Series Technical Datasheet 2017.pdf [383.42 KB]
PM3200, PM3210 Installation Guide 2019.pdf [3.66 MB]