המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why OFS configurator is only in English on 3.62 version?
Issue
OFS DA configurator cannot be changed in French or German with OFS 3.62

Product Line
OFS DA

Environment
From version 3.62

Resolution
Since OFS DA 3.62, the OFS configurator is available only in English. This feature has been removed and not supported anymore because OFS server and other tools are since the beginning only in English.
Therefor, OFS configurator has been set only in English.