המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does LINK150/EGX150 have conformal coating applied to its circuit board?
Issue
ION meters contain conformal coating on its circuit boards. Does LINK150 or EGX150’s circuit board have such coating on their Printed Circuit Boards (PCB)?

Environment
LINK 150 or EGX 150.

Cause
Conformal coating is a protective coating or polymer film that 'conforms' to the circuit board topology. Its purpose is to protect electronic circuits from harsh environments that may contain high humidity, a range of airborne contaminants and varying temperatures.

Resolution
LINK150’s PCBs (Printed Circuit Board) have conformal coating on it; the variant that has been used is AB Chimie.