איך נוכל לעזור לך היום?

EcoStruxure Hybrid DCS 2019: How to create an Expression based on Folder Hierarchy

Goal:

This Video explains the procedure to create an expression based on Folder Hierarchy.

Product Line:

Ecostruxure Hybrid DCS2019

Environment:

Windows 10, Windows Server 2012R2

Procedure:

In Previous versions of EHDCS, Automatic bulk creation of Sections is based on the instance name and will create a section per instance. In EHDCS 2019, User can configure their own expression for Automatic bulk assignment and creation of sections in control project. The below procedure shows how to create an expression based on the Folder Hierarchy.