המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
how to create a Web Dsigner application for the BMENOC0311 Factorycast module.

Issue
The purpose of this video is to demonstrate how to create a Web Designer application for the BMENOC0311 Factorycast module. The video also demonstrates how to create the Unity export file that is required for importing the variables into the Web Designer application during development. The user must be familiar with using both Unity and Web Designer.

Product Line
BMENOC0311

Environment
Windows 10

Resolution
The purpose of this video is to demonstrate how to create a Web Designer application for the BMENOC0311 Factorycast module. The video also demonstrates how to create the Unity export file that is required for importing the variables into the Web Designer application during development. The user must be familiar with using both Unity and Web Designer.