המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Download links for Vijeo Designer V6.2 SP10
Issue:
Where can we find the download links for Vijeo Designer V6.2 SP10?

Product Line:
Vijeo Designer V6.2 (all hotfixes and service pack revisions less than SP10)

Resolution:
Please find the download links for Vijeo Designer V6.2 SP10 attached to this FAQ at the bottom of this article.
(Updated 2023-02-21)

You must have Vijeo Designer 6.2 already installed.
Each SP is cumulative, so you do not need to install SP1-9 first.
*NOTE: In order to successfully install the service pack or any of the related packages, always right-click on the exe file and select "Run as Administrator". This will ensure the installation is completed properly.

(Required updates)
1) Just the patch to install on top of the existing Vijeo Designer v6.2 installed on your PC/laptop for the Development Environment (341MB):
"Vijeo_Designer_Development_SP10(6.2.10.23_6.2.10.21).zip"

(Optional updates)
2) Help files update to your Vijeo Designer v6.2 (Vijeo Designer HTML help files and PDF manuals) - 1146MB:
"SP10_Docs_Pack(6.2.10.23_6.2.10.21).zip"

3) iPC/Standard PC Runtime if you need to have an iPC/Standard PC running as an HMI by itself - 66MB:
"Runtime_For_Windows_SP10(6.2.10.23_6.2.10.21).zip"

4) Data Manager for retrieving Logging/Recipe data from an HMI (this is installed on your laptop/PC on top of your existing Vijeo Designer v6.2) - 61MB:
"DataManager_SP10(6.2.10.23_6.2.10.21).zip"

5) Web Gate Client Files (this is for if you are connecting to the HMI and want to mirror the screen on a remote PC's browser) - 19MB:
"Web_Gate_Client_Files_SP10(6.2.10.23_6.2.10.21).zip"

שניידר אלקטריק ישראל

קבצים מצורפים
SP10_Docs_Pack(6.2.10.23_6.2.10.21).zip [1.09 GB]
DataManager_SP10(6.2.10.23_6.2.10.21).zip [59.68 MB]
Runtime_For_Windows_SP10(6.2.10.23_6.2.10.21).zip [64.62 MB]
Web_Gate_Client_Files_SP10(6.2.10.23_6.2.10.21).zip [19.04 MB]
Vijeo_Designer_Development_SP10(6.2.10.23_6.2.10.21).zip [340.79 MB]