המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Does Vijeo Designer support Siemens TIA Portal V16?
Issue:
Unable to communicate with a PLC programmedwith Siemens TIA Portal V16 using a Magelis HMI programmed with Vijeo Designer

Product Line:
Vijeo Designer, Magelis, XBTGT, HMIGTO, HMIGTU, HMIGK, HMISTU, HMISTO, iPC

Resolution:
The ability to import symbols and the ability communicate to a PLC programmed with Siemens TIA Portal V11 - V15 is now available in Vijeo Designer 6.2 Service Pack 10. Starting from Vijeo Designer 6.2 Service Pack 11, support for TIA Portal V16 will be added. This version will be available at the end of January 2021.