המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to use web browser in EOTE on HMIST6 series
  1. Issue
How to use web browser in EOTE on HMIST6 series? Is it possible to use in simulation mode?
  1. Environment
EOTE V3.1
  1. Resolution
Only HMI target with windows based operating system(HMIG5U or HMIG5U2) supports web browser. Since HMIST6 is not windows based, EOTE on HMIST6 series does not support web browser. In addition, web browser feature is not supported in the simulation mode. You can only use it during EOTE runtime.

  1. FAQ Applicable Conditions
FAQ also applies to EOTE V3.1 SP1.