המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the limit for imported variables in a Web Designer project.
Issue
What is the limit for imported variables in a Web Designer project.

Product Line
Web Designer

Environment
Windows 7, windows 10

Resolution
The maximum number of WORD type variables that can be defined in a Web Designer application for a Factorycast module (i.e., BMXNOE0110, BMENOC0311, BMENOC0321) is 1000.  If STRING type variables are used, the  device 'Variables' table namespace in a Web Designer application for a Factorycast module is limited to a total of 2000 bytes.  If the 'Variables' table contains a mixture of WORD and STRING type variables, the limit is still 2000 bytes.   Any attempt to exceed the limit could result in communications issues with the Web Designer services.


This limit is due to the available memory in the module and cannot be changed.