איך נוכל לעזור לך היום?

Is it possible to define an AXIref in M580 safety CPU?

With CE V14.1 and previous versions it was not possible to define an AXISref for all M580 safety CPU.
With CE V15 it would be possible (a fix will be delivered for that).
(AXISref is required for using MFB in motion PLC applications).