איך נוכל לעזור לך היום?

Can I use voltage signal on AI3 of the ATV320?

Issue:
Customer has 40Vdc input connected on AI3 analog input of ATV320.

Product Line:
ATV320

Environment:
All model numbers, all serial numbers

Cause:
ATV320 didn't follow the voltage input signal on AI3

Resolution:
No, AI3 input of the ATV320 only accept 0-20mA or 4-20mA current signal.