איך נוכל לעזור לך היום?

BMXCRA312x0 and the BMECRA312x0 remote adapters 'Custom RPI' parameters settings does not work.

Custom RPI settings for the BMXCRA312x0 or BMECRA312x0 remote adapters do not work when using Unity V13.1, CE V14.0, or CE V14.1.

For example, if the RPI is set to 31ms in the following configuration,


The RPI does not display the change in the DTM.


The issue is resolved in:
  • Control Expert V15.0
  • Control Expert V14.1 using HotFix1 (HF1)