איך נוכל לעזור לך היום?

EcoStruxure Process Expert [2020R2] Switching from Safety mode to Maintenance mode in M580 Safety online refinement

In order to perform modifications in online refinement of a M580 safety controller, User must switch the Safety mode to Maintenance mode. By default, the online refinement will be opened in Safety mode only.

For switching the mode from Safety to Maintenance from Controller tab, the Safety/Maintenance button is disabled in refinement of EPE2020R2.

pic1

User must use the Safety button provide at right top corner as shown in the below picture.

pic2

After clicking on Safety button, if Password is enabled, then system will prompt for security password and after successful entry of correct password the mode will be changed to Maintenance mode.
In case of User had disabled the Password protection, the mode will change from safety to Maintenance upon clicking the Safety button.

This document is applicable for Ecostruxure Process Expert 2020 R2 Software.