איך נוכל לעזור לך היום?

What is the mounting base for 171CBU98090?

The Momentum Processor is a (top hat) and it has to be mounted on an I/O base that provides the power to the processor, you can have an analog or discrete base under it depending on the needs of the user.