איך נוכל לעזור לך היום?

How to use FanIn function while developing template in Ecostruxure Process Expert

As a User of Ecostruxure Process Expert template, I want to know the behavior of FanIn when it is connected to parameter, interface, input values so that it reduces the understanding gap while developing templates in Ecostruxure Process Expert.

Step 1: When in template editor, Navigate to Toolbox and then in Functions section drag and drop the FanIn into template editor.
image1
Step 2: On right click of Mouse on FanIn, there are multiple options one of them is extend operation which will allow user to configure multiple inputs to FanIn function.
image2
Step 3: For this example, we shall have 3 additional inputs. (Maximum 10 inputs are supported)
image3
Step 4: On right click of mouse on In, we get multiple options . When we click “Create Input Value” , it will bind hardcoded value to the input. Other options for binding are parameter, Interface, other elements.
image4
Step 5: We have configured the function as below
image5

FanIn function: The output will have the string value of Input depending on priority. First being In and then In.1 and so on.
Scenario 1: When the interface is connected and value is passed at In then Out will have value of In
Scenario 2 : When the interface is not connected so there is no value at In then the next priority would be In.1 . If the parameter has a value then Out will have value of In.1
Scenario 3 : When the interface is not connected so there is no value at In then the next priority would be In.1 . If the parameter also has no value then the next priority would be In.2 ,important to note here that Out will have value of In.2 irrespective of the input field has value or not, due to hard binding(Constant) with input value.