איך נוכל לעזור לך היום?

Ecostruxure Automation Expert [21.1]: How to read Real Time Clock from Controller.

User can read Real Time Clock from Controller by using a Function block MIBGET. This Function block is available in service section of Runtime.Base library.

MIBGET function block is internally used for getting diagnostic information.

Provide a constant with string 'System.CurrentTime' at Path1. Create a Constant at Q1 and make it True.

pic1

After deployment to Controller, you can see, the block had read the system time and was available at Value1 output.

pic2