איך נוכל לעזור לך היום?

Where must the wiring kit be connected in PrismaSeT Active?

You can connect the wiring kit upstream or downstream. Today, 90% of wiring kits connections are downstream.

The purpose of the wiring kit is to make sure that the wireless panel server is correctly connected with the right protection.
image.png

If you need to connect the wiring kit upstream, we highly recommend that you use an additional protection that can be opened during maintenance (without cutting off the power).

If you are looking for further information regarding the steps to follow when installing the wiring kit, watch this video:
https://www.youtube.com/watch?v=Du8xGHIu9M4

You can also access this instruction sheet:
https://download.schneider-electric.com/files?p_enDocType=Instruction+sheet&p_File_Name=NNZ50846-01.pdf&p_Doc_Ref=NNZ50846