Why is my M580 stopped after a loss of power?
Issue
PLC is stopped after loss of power
Product Line
M580
Environment
EcoStruxure Control Expert
Resolution
The CPU will only go back into run if you have Automatic start in Run checked off in the configuration. Otherwise it will be stopped when power is restored.
פורסם עבור: שניידר אלקטריק ישראל